This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1606: Maximum data rate to FPGA

Genius 17665 points
Part Number: ADS1606

Hi Experts,

Good day.

I am using ADS1606 in my design. In the datasheet the sampling rate is mentioned as 5MSPS.

I just want to know at what max speed or data rate I can transfer the data from the ADC (Parallel data) to my FPGA.

Also, seems this device has no EVM, can you provide alternative evaluation for this?

Thank you in advance.

Regards,
Archie A.

  • Hello Archie,

    I assume the customer wants to know the maximum /RD frequency when using the FIFO.  In this case, the maximum speed that data can be transferred from the ADS1606 will be 50MHz, determined by t-18=10ns and t-19=10ns in Figure 4.

    ADS1606 no longer has an EVM available and we do not have any other hardware platforms available for this device.

    Regards,
    Keith Nicholas
    Precision ADC Applications