Part Number: ADS5294
Hi team,
ADS5263 Reading PHASE_DDR Register
One of our customers is experiencing the following issue, which is similar to the issue in the link above, but no resolution is given above.
This customer using the ADS5294 occasionally get a clock 8 channel full data error in test patterns mode. An attempt was made to modify ADDR 0x42H [D6:D5], but it was read out as 10, indicating a write failure. What are the prerequisites for reading and writing this register?
Best Regards,
Amy Luo