Hi,
My customer is using ADS1000A0IDBVT to send the digital value the uP when a certain device is connected or disconnected. When the temperature of the ADC rise to ~ 50 degree C, the ADC starts railing to full scale causing false detection. The ADC is rated for 125 degree C. Do you have an explanation to what could be happening with the ADC?
Thank you.
Regards,
May