Part Number: AFE4950EVM
Other Parts Discussed in Thread: AFE4950
Hello
This is a question related to AFE4950EVM
1. In "AFE4950_Register_Generation_v2.1_PPG_ECG.xlsm",
what does the different color of the Reg map mean?
light blue, light orange, light yellow, orange, etc.
2. After importing the default .cfg file...
When Capture is executed in the GUI, is the raw data displayed on the GUI screen coming out through 0x6D READ_POINTER?
Or is there a separate register that outputs raw data?
3. Is it possible to provide a reference code for the provided GUI program like the previously provided MSP firmware?
(It only asks if this is possible.)