Hello,
The datasheet described the Do's and Don'ts (continued) at 10.3 chapter, it didn't allow to connect inductor between VCC and GND. Could you please help to describe what is the reason?
One customer used 5V to 3.3V output , the output has connected ferrite bead, and found that there is ripple of the 3.3V which is fed to ADS1248, and it caused the ADS1248 couldn't work normally。If remove the ferrite bead, the ripple disappear. That is why we asked the ADS1248 datasheet about the Do's and Don'ts (continued) at 10.3 chapter description.


Best regards
kailyn