Other Parts Discussed in Thread: ADS7828
We have a question on power-on sequence on ADS7828.
In our case, 8ch analog inputs are used for monitoring various analog DC signals.
During power-on sequence on ADS7828, some of these monitoring signals are already active before VDD supply.
That means, strictly speaking, analog inputs would be over VDD+0.3V in booting, because VDD starts from GND in power on.
Would ADS7828 accept such over-voltage input conditions in power on sequence?
According to absolute maximum ratings, digital input voltage to GND doesn’t allow to over VDD +0.3V.