Part Number: ADS8904B
We are considering new adoption of ADS8904B.
From the specifications of the product under development, the ADC is single-ended input.
SAR with high resolution (19bit or more) is required.
I would like to use the ADS8904B with the following inputs, is there any problem?
・REFIN:4.7Vref input
・REFM:to GND
・AINP:0~5V input
・AINM:to GND
Sorry for the vague question.