I am able to record data using My ADS1198 based circuit.
I have ADS1198PDK as well.
The data i am receiving is noisy in nature, they are not clean. (See the attached Image).
Even the * channel that i am receiving is noisy.
Only Lead 1 data signal is clean otherwise all are noisy.
I have power taken care of power requirement as per datasheet, providing power supply using a 5V adapter.
So, help me with clearing the signal.
what can i do to have noise free signals.
Thanks.