Other Parts Discussed in Thread: TMS570LS3137, ADS1278, THS4524
Hello Team,
I am trying to connect the ADS1278 with TMS570LS3137 MibSPI, I am seeing some inconsistence output from SPI Output.
My setup is i am driving the ADC with 2V input with THS4524 and measured voltage level at ADC pins Input differential level is 2V and its stable too.
For all 8 channels are in 2V input. I am trying to read the data from SPI and I am seeing below behavior,
From channel-01 I am getting stable output (2V) when I read from Debugger Mode, but for 10 readings once I can see some deviations like 1.5V or 0.8V. but Analog input is still stable at 2V.
For Channels-03 to 04 I am getting deviations in outputs for 3 or 4 readings. But other channels-05 to 08 not getting the consistency output from SPI Data and lot of deviations like its showing negative values sometime since my input is at 2V.
Please let me know can I get some assist to resolve this issue?
Thanks,
Venugopal