Part Number: ADS1263
Hello,
I am writing a library for the ADC circuit and wanted to clarify if I understood the datasheet correctly. There are three questions in different aspects of the chip.
1. Correlation between Data Rate, Sinc Filter, and conversion latency
I think I understand that the data rate is determined by the clock frequency and the decimation of the first and second digital filters. I am a little confused about the Data rate from 14400 to 38400 SPS. When I select these sampling rates by changing DR[3:0], does the second filter gets bypassed internally to meet the sampling rate, regardless of FILTER[2:0] bits? And does this also mean the conversion latency becomes only SINC5 amount listed in tables 9-13 in the datasheet?
After the first conversion with the latency provided by table 9-13, it says the subsequent conversion occurs at a nominal data rate. Does this mean, for example at 38400SPS, the first conversion happens 0.207ms but the next conversion is going to happen at 1/38400, in continuous conversion mode?
2. When CRC bits are set to enable either CRC or Checksum, does this introduce any delay in conversion or data transmission compare to when it's disabled ?
Thanks,
Steven