Part Number: ADS1299EEGFE-PDK
Other Parts Discussed in Thread: ADS1299
Hello,
One customer used the ADS1299 for his application, when debugging the ADS1299, there was a collision between the acquisition function and the electrode-off detection function, which showed that when he turned on the electrode-off detection function, the CMRR fell from 120dB to around 90dB. What is the problem?
Note: 500Hz sampling rate, 2.048Mhz external clock.
Best regards
Kailyn