Hi Experts,
Good Day
I hope you're doing fine.
I need your help. One of our customers is asking below setting.
Question 1) If K=8 in the FRAMES PER MULT IFRAME field of register 31, does the LMFC count range from 0 to 8, and when it reaches 8, does it become 0? Or is LMFC always 0-31?
Question 2) When the LMFC count ranges from 0 to 8. Listed in register 3C. There is a description "the LMFC count resets to 0 and K28.5 stops transmitting when the LMFC count reaches 31.", but if the LMFC count does not reach 31, will K28.5 continue to output?
Thank you
Regards,
Josel Go