Two questions regarding this note in the datasheet (Applications Information -> Reference Circuit):
"The external reference driving circuit should be designed to provide the required switching current for the eight ADCs inside the chip."
1. Is there a bandwidth requirement imposed on this switching current? (based on maybe sample rate or signal BW)
2. There is no min/max spec. for switching current, only a typ. Any advice on margin/overhead?