Other Parts Discussed in Thread: ADC3644EVM
Hi,
Good Day. It is regards to the forum post below.
It is said that the schematic diagram of ADC3644EVM is the same to ADC3662EVM.
We don't understand how these two components are pin compatible. DCLKIN for the two components don't match up.
ADS364X: DCLKIN goes to package pin 33. ADS366X: DCLKIN first off is differential. It uses package pins 24 and 25.
If both EVM are not compatible, can we have the schematic diagram of ADS3662EVM?
Please advise. Thank you very much.
Best Regards,
Ray Vincent