Other Parts Discussed in Thread: ADS8166, ADS8168EVM-PDK
hello team,
I use ADS8166 to convert 8 channels(From AIN0 to AIN7 auto sequence mode), and I find if just AIN0 is added on some voltage(2.048V) , after converting, we can see AIN0 is 32768, AIN1 is also with some value, nearly 100, but AIN2 is nearly 0.
And also , I do another test; just AIN1 is added on some voltage(2.048V), we can find AIN2 has some value, AIN3 is nearly 0.
And so on......
So, I guess the continuous 2 conversions, the 2nd convert shall be influenced by the 1st convert ?
So, if you have some experience about it ?
Pls give me some advices, thanks a lot!
BR