This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200QML-SP: SYNCSE timing requirement - Subclass 0 (No SYSREF)

Part Number: ADC12DJ3200QML-SP

Hello, 

My application will use the ADC12DJ3200QML in JMODE0 (single-channel) and subclass 0 (single device, no SYSREF synchronization).

According to ADC datasheet, the JESD204B synchronization is initiated by the FPGA (data receiver) through the assertion of the SYNCSE (or TMSTP+/-) signal with the setup/hold requirements with respect to multi-frame boundary (figure 6-1).

In my subclass 0 application, there is no SYSREF clock allowing my receiver receiver FPGA to know the multi-frame boundary.

I suppose I have to determine the multi-frame boundary through my JESD204B FPGA core and thereby meet the SYNC setup/hold requirements correct ? 

Should I instead initiate the JESD204B synchronization through the SPI bus ? It would be simpler.  

Thanks