This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RF: data mapping on link layer

Part Number: ADC12DJ5200RF


Hi,

I'm a bit confused about the sample or data mapping on the JESD204B link layer.

The link layer is always 256bit width. 

I like to check how was the data mapped at link layer output in JMODE0/2 and JMODE11/22 (most wanted). Thank you.

Regards,

Ying

  • Ying,

    We are looking into this.

    Regards,

    Jim

  • Hi Ying,

    Table 7-27,7-29,7-36 and table 7-45 show you the data packing for JMODE0,2,11 and 22.

    Regards,

    Neeraj

  • Hi Neeraj,

    My question is how were the data on Table 7-36 and Table 7-45 mapped onto JESD204B link layer. It's a 256bit bus. Thank you.

  • Hi Jim,

    Any updates? Hope to hear from you ASAP. Thank you.

  • Hi Jim,

    Any updates? Thank you.

  • Hi Ying,

    The Xilinx JESD IP does the following:

    1> It concatenates the data of all the lanes to generate one output bus. For an 8 lane link, you will see a 256 bit bus (32 bits per lane per clock cycle)

    2> On each bus, the order of the bytes is reversed (to ensure that the first received byte is mapped to byte 0, the second to byte 1 and so on).

    To map the JESD IP output to the data you see in the JMODE table, kindly do the following:

    1> Separate the 256 bit bus into 8 32 bit segments. The lowest segment (31:0) will be for Lane 0, the highest (255:224) will be for Lane 7

    2> For each lane, byte reverse the data. You should now see the data map exactly as displayed in the JMODE table. Please note that in cases like JMODE0, where F=8, you need to accumulate two cycles of data on each lane (to create the 64 bit frame) in order to check the mapping of the data to the JMODE table. The 64 bit frame is also needed in order to identify the correct 4 tail bits that need to be discarded in each frame.

    I hope this addresses your query.


    Regards,

    Ameet