Part Number: AMC7836EVM
Other Parts Discussed in Thread: AMC7836
In my lab, amc7836 evm board works in the clamp output mode,the clamp voltage is -10 v;
And when the clamp output‘s ’load current is -4mA,the the clamp voltage is still -10 v;
But in the datasheet,clamp output impedance typtical value is 8kohm, the max load current should be -10v/8kohm=-1.25mA,
so what's the reason that in fact I can drive the clamp output to -4mA?