Part Number: ADS1675REF
Other Parts Discussed in Thread: THS4503
Hi,
Good Day.
Customer is using an ADS1675REF board. He is wondering what the current limit to expect/set on the analog input +5V driver is?
Section 3.2 of the manual: "The ADS1675REF board requires an independent analog +5V supply to power the analog portion of the device under test, the external reference, and the external reference buffer, as well as provide the amplifier common-mode voltage. This voltage is applied to J5 pin 3 and is denoted as +5VA. This supply can be monitored at TP7"
This is the driver for the +-2.5V differential analog input. So a power supply not a signal input?
Please advise. Thank you very much.
Best Regards,
Ray Vincent