If only 1 channel is used by an application, how to treat the remaining two differential outputs pins of the second channel?
Is it OK to leave them unconnected or do they need a different treatment?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If only 1 channel is used by an application, how to treat the remaining two differential outputs pins of the second channel?
Is it OK to leave them unconnected or do they need a different treatment?
Hi Walter,
I would put a 100ohm pullup to AVDD as shown in the datasheet, then put a 0.1uF cap to ground on each analog output.
Regards,
Rob