Part Number: ADS1278-SP
Hello,
We are using the ADS1278WHFQ-MLS adc converter and need to understand the impact of operating below the AVDD min of 4.75V spec. Can you provide any insight?
This is difficult to hold in our design, which uses a SMPS to generate 5.2V +/- 1.62% RSS… passed through an LDO (TI TPS73801MDCQPSEP) to clean it up but with .35V dropout and tol of +/- 2.73% RSS.
SMPS tol : 5.2 – 1.6% = 5.12V
LDO dropout: 5.12V - .35V = 4.77V
LDO tol: 4.77V – 2.73% = 4.64V
This leaves 4.64V for AVDD at ADC… which falls below the 4.75V spec.
I cannot easily move the SMPS set point up as it’s a Crane module, already built.
I could change to an LDO with even lower dropout requirement, if such a beast exists for space.
Otherwise, if the 4.75V min for AVDD is real, I’ll need to replace LDO with an RLC filter to cleanup the SMPS output and feed filtered to AVDD.
Thanks,
Adam