Part Number: ADS7883
Other Parts Discussed in Thread: ADS7886,
Hi Team,
We are looking for an ADC with the following specifications.
Min value of SCLK of ADS7883 and ADS7886 is not specified.
Can I use it with “SCLK=50Hz”?
And, could you please let us know if you have any recommended device?
<ADS7883>
<ADS7886>
<Specification>
Power supply:+5VDC
Analog input:0 to 5V
Input channel:1ch
Bit number:more than 12bit(12 to 16bit)
TA:-40 to 105℃
Output:SPI
SCLK is 50Hz
Regards,
Hide