Part Number: DAC81404
Hello,
In my application I want to use a daisy-chain of four DAC81404.
I will only perform write operations, no readback.
In this case, which of the timing specs from the datasheet apply?
"Read and Daisy Chain" as per table 7.8-7.11
or
"Write" as per table 7.6 and 7.7
Do I understand the wording correctly, that "Read and Daisy Chain" includes these 3 cases:
- reading without daisy-chain
- reading with daisy-chain
- writing with daisy-chain
and "Write" means only writing without daisy chain?
I am not sure I understand the wording unambigously.
Thanks in advance for the help.
Regards,
Marcel