Part Number: ADC08500
What is the maximum LVDS clock input for ADC08500? The datasheet does not specify maximum value, only operating frequency of 500MHz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC08500
What is the maximum LVDS clock input for ADC08500? The datasheet does not specify maximum value, only operating frequency of 500MHz.
Hi Bob,
The maximum clock signal level can be determined by the operation conditions table in the datasheet.
So LVDS will work, which is typically 800mVpp DIFF.
See below.
Thanks,
Rob
Hi Bob,
The max sampling rate of the ADC is 500MHz. Therefore, the clock input rating is 500MHz.
Regards,
Rob