Hi sir/Madam.,
I am planning to select one ADC for below specifications for RF Detector Voltage Monitoring application.
1. Input DC voltage to ADC - 50mV(Min)
2. Input DC Voltage to ADC - 3400mV(Max)
Input voltage to ADC will be varying depend on RF signal from minimum to maximum . Kindly help me on this for selecting ADC or suggest some part for the same.