Part Number: ADS5294
Hi,
We are using single device ADS5294, no decimation. Our sampling frequency is 10Mhz, 2-wire mode.
We want to output a single pattern.
We did the experiment with external sync: Steps we followed:
1. Soft RST( configure registers after RST)
2. EN_SYNC in ADC
3. TP_HARD_SYNC Enabled along with the test patterns
4. send a hard sync pulse
5. Write single custom pattern
6. enable SINGLE_CUSTOM_PAT
what is the correct way to go back from test mode to acquiring real samples
Just turn off/disable SINGLE_CUSTOM_PAT only or disable 2 and 3 as well above?
LT