Other Parts Discussed in Thread: THS8200
Hello,
I am trying to set up the THS8200 to output a 640x480 VGA signal. The THS8200 is working along with an LCD Controller in the NXP LPC2478 ARM7 Processor. The LCD controller outputs 24 bit RGB signals along with H-sync and V-sync data and a clock of 24MHz. Everything looks right on the digital side of the circuit as far as we can tell. Right now, it seems there is a synching problem. For example, when I try to display a single vertical line, the line is repeated about 10 times and slopes diagonally from top right to bottom left. Currently, the registers we have set are:
Sub-address; value
0x03; 0xC1
0x19; 0x03
0x1C; 0x70
0x34; 0x03
0x35; 0x20
0x36; 0x00
0x37; 0x01
0x38; 0x87
0x39; 0x22
0x3A; 0x0D
0x3B; 0x0D
0x3C; 0x80
0x4A; 0x8C
0x4B; 0x44
0x4C; 0x00
0x4D; 0x00
0x4E; 0x00
0x4F; 0xC0
0x70; 0x60
0x71; 0x00
0x72; 0x01
0x73; 0x03
0x74; 0x00
0x75; 0x01
0x76; 0x00
0x77; 0x07
0x78; 0xFF
0x79; 0x00
0x7A; 0x00
0x7B; 0x00
0x7C; 0x00
0x82; 0x43
If anyone has any advice to help resolve this problem. Please let us know.
Thank you.