This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS114S08EVM: Does ADS114S08EVM support single end measurement?

Part Number: ADS114S08EVM

Does ADS114S08EVM support single end measurement? If yes, how to configure the registers to read for example channel 0?

Thanks

  • Hi Jennifer,

    Welcome to the E2E forum!  The intention of the EVM is to show multiple types of sensor input connections to include RTDs, thermocouples, thermistors, bridge sensors as well as voltage and current measurements.  For the voltage and current measurements J9 is used for the input connections and is explained in section 5.1.3 of the ADS114S08EVM User's Guide.  Table 14 shows the various input voltage connections that can be used and the jumper selections required for those measurements. 

    There is a basic startup script for making these measurements in the software GUI by selecting the appropriate script and running it.

    Best regards,

    Bob B

  • Thanks. This resolved my issue.