Part Number: DAC161P997
Hello Everyone,
I hope you all are fine and doing well. I am planning to use DAC161P997 in one of my design to produce accurate 4-20mA output. I have used the same reference circuit given in the datasheet. But it is giving Fix Current output 11.8 mA with Zero DAC Code and 14.6mA output with any DAC Code Other than Zero(Between 0 and 65535). Below are some key points which I have observed.
1. My Digital communication seems ok as I am sending DAC Code every 500ms and I am observing High to Low transition on Ack Pin after the end of frame of each DAC Code.
2. Also There is no error(Error Pin is always high).
3. The loop also seems ok as I am getting -600mV across the Out Pin of DAC and (COMA/COMD).
Please suggest what other things may be there which I am missing.
Best Regards,
Karan Thawani