Other Parts Discussed in Thread: ADS1256
I have a customer with the following issue below. Please advise.
I am using TI’s 23-bit ADC, ADS1256IDB, and have some conversion problems. If I lower the sampling rate to get better accuracy, the results are wildly inconsistent below the 1 kS/s setting. I am using a 6.25 MHz clock, so the sampling rate scales as 6.25 / 7.68 * SR. I have also slowed the switching time between inputs as I do this. Six of the inputs are tied to an amplified ground signal, so 0 V plus any offset and noise, and the seventh input is tied to a 2.5 V reference. None of these signals are changing except of the small amount of noise on any.