Other Parts Discussed in Thread: ADS54J69
The TI-JESD204-IP documentation specifies that the RX_LN_DATA_WIDTH parameter has only the following valid options: 32, 64, and 128 bits.
However, I want to run the ADS54J69 using 4 lanes at 4.9152 Gbps which according to its data sheet (see figure 74 on page 36) has a lane data width of 16-bits.
Is there a way to configure the TI-JESD204-IP to support this mode or do I need to use another JESD204 IP (possibly from Xilinx)?
Thanks.