Part Number: DAC81408EVM
I have been using this DAC-EVM for some time, and all the ports were working fine. Recently I see that THREE out of EIGHT channels are not working.
Channels 02, 06 and 07 are giving voltages -10V, -10V and 10V respectively. My VSS and VCC voltages are -10 V and 10 V, for I am using them at ±10V range operation.
Could this be a hardware problem?
Did anyone experience multiple channel failures before?
Codes are proper, all registers are set properly. And these channels worked before. Hence I am ruling out script errors from the list of causes.
I am using code functions from Matlab via RaspberryPi for programming.