This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7953-Q1: Input Signal Absolute Maximum Current Limit

Part Number: ADS7953-Q1

Hi team,

Reviewing the ADS7953-Q1 datasheet and noticed there was no Abs. Max value for current into the device inputs. Usually there is some guidance. I've seen a lot that are usually ~2mA.

What's the abs max current limit for the signal input of the ADS7953-Q1?

Thanks,

Jacob

  • Hi Jacob,

    I think the general guidance here is to keep the analog input current < 10mA. Any higher and damage to the input ESD diode structure may occur. Additionally, continuous usage at 10mA may cause long term reliability issues. 

    Regards,
    Aaron Estrada