Part Number: ADS1015
Hello Experts,
I have been doing some testing with the ADS1015 and was wondering at what voltage past VDD I should start to see data inaccuracy of an analog input. The data sheet states under the recommended operating conditions that the voltage of an analog input should not exceed VDD. The data sheet also states that the max rating is VDD +0.3V. Keeping this in mind, I have been testing up to VDD +0.3V and have not experienced data inaccuracy. I have mainly been testing the analog inputs from 2.8-(3.2 or 3.6)V with a full scale range of 4.096V. Any information would be greatly appreciated.
Thanks,
Matt M