Part Number: ADS8686S
Hello
I need help in locating Bipolar Input ADC's such as those similar or
equivalent to AD7616, AD7617
Maybe you can consider this as a suggestion.
While looking for the equivalent of the above I cam across this P/N ADS8686S
This is listed under Precision ADC's.
Most are Unipolar Inputs while I was looking for Bipolar Inputs.
The Parametric Table doesn't have a column for Input Range ;
at least I couldn't find one for say -10V to +10V Input, 12 to 16 Bit, 12 Ch or more.
If the Parametric Table can be configured to include this feature, would make it
so much easier to find
Thanks and with best regards
Varun