Part Number: ADS4149
Hello,
We are using hardware which implements a 208 MHz LVDS DDR data interface between the ADS4149IRGZT and an FPGA. We have a version of the board which was only modified by skewing phase by 80 ps on the input data clock. We now have had to adjust timing constraints in the FPGA and ADC register settings in order to get DDR data clocking into the FPGA correctly. Are there any known cases in which adjusting the delay on the input clock also changes the characteristics of the output clock? With respect to a shift of the output data clock relative to the output data, not overall system latency.