Part Number: ADS8684
Other Parts Discussed in Thread: ADS8688
HI.
I have a question on the ADS8684.
When a surge is applied during EMC test, the AVDD voltage used in ADS8688 drops from 5V to 3V.
So the register is not written.
Even after reset using the reset pin, AVDD is still 3V.
If both DVDD and AVDD power of ADS8684 are turned off and on again, it will return to normal.
In addition, as a result of checking the power supply, It was confirmed that 100mA was used more when the surge was applied.
*I think the AVDD voltage goes down by using more AVDD current in the ADS8684 IC.
Have you ever had something like this happen?
Also, please suggest a solution
thank you
*LT1461 (Micropower Precision Low Dropout Series Voltage Reference Family) IC is used to supply AVDD voltage.