We would like to use the DAC12DL3200EVM with both channels being DC coupled. We saw from the schematic that the board is shipped AC transformer coupled. Is there a way we can change the assembled components on the PCB (namely the L1,L2,L3,L4 and AC coupling capacitors, and transformers or any other you suggest) to convert the output to DC coupling single ended? Please note that our maximum frequency is 150 MHz on each of the two channels working with 600 MHz sampling rate. In case of positive answer did you ever test such configuration? Do you have any measurement result with DC coupling to share?
Thanks and kind regards
Luca