I am looking for ADC to meet the following specification( Test/Measurement application):
1.Analog Bandwidth --> 20 MHz+
2.Sampling rate--> 10Msps to 100Msps
2.ADC resolution --> 10bits+
3.Channels --> 2(BNC/SMA)
4.Input range -->up to 80V(external divider)
Please review the requirements and let us know the suitable solution from TI.
Please let me know if there are available modules to meet the req.
Regards,
Venu