This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8760: Probable solution mistake in ±12VDC supplied DAC because positive output control isn´t possible?

Part Number: DAC8760

Hi,

We have used DAC8760 converter earlier with unipolar supply (24VDC) and it has worked well.

Now we utilize this very same circuit for another application having ±12VDC supply. Below is schematics of the design.
Currently we have faced issues with positive output voltage control. Negative side of VOUT is working perfectly but positive VOUT gives
only 0,7V maximum. Could there be somekind of schematical mistake made?