This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC37J82:DAC_PLL、Serdes_PLLのLOCK信号について

Part Number: DAC37J82


内蔵 PLLについて教えてください。
DAC_PLL、Serdes_PLL
どちらも一度クロックを停止して
クロック周波数の変更を行っいます。
この時の、DAC_PLL、Serdes_PLLのLOCK時間を教えてください。

入力クロックのジッタは規格内とします。

また、LOCK信号が遅くなる要因は何があるのでしょうか?

(1)この時の、DAC_PLL、Serdes_PLLのLOCK時間を教えてください。
(2)LOCK信号が遅くなる要因は何があるのでしょうか?

  • Please send your complete issue in English. We cannot read this post.

  • I'm sorry. Please tell me about the built-in PLL. DAC_PLL, Serdes_PLL Both stop the clock once Change the clock frequency. Please tell me the LOCK time of DAC_PLL and Serdes_PLL at this time. Input clock jitter should be within specification. Also, what are the factors that slow down the LOCK signal? (1) Please tell me the LOCK time of DAC_PLL and Serdes_PLL at this time. (2) What is the factor that slows down the LOCK signal?

  • Yamauchi

    This has not been measured. There are serval register writes required to get the PLL and serdes PLL to lock and another register read to get the lock status. The DAC PLL also requires to be tuned based on the reference clock and output frequency selected. This will take several spi writes. The SPI speed is the major delay related to the required lock time.

    Regards,

    Jim