This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3422: Interface it with a spartan 6 FPGA

Part Number: ADC3422


Hi Team,

Good day! Our customer is asking how ADC3422 can be interface with a spartan 6 FPGA.  If possible could you please provide Verilog files or some project for ADC3422? 

Thank you so much in advance.

Best regards,

Jonathan

  • Hi Jonathan,

    We don't have any project files available for the Spartan 6 FPGA. The capture board (TSW1400EVM) which the ADC3422EVM interfaces with is an altera. I would suggest the customer ask Xilinx on the best approach on how to implement a 4 or 8 pair LVDS interface (based on whether they want to use the ADC in 1-wire (4 LVDS pairs) or 2-wire (8 LVDS pairs) mode) on the Spartan 6 FPGA. Keep in mind that since this is Serial LVDS (SLVDS), the frame clock (FCLK) is used to indicate the transition/partition between each sample. Also, the data clock is DDR, meaning the data is valid on both the rising and falling edges of the data clock signal.

    Regards, Chase

  • Hi Chase,

    Thank you so much for your suggestion and information! It really helps. Would you mind to share the Verilog files of using ADC3422(interfacing with an altera is okay)? Thank you again and have a great day.

    Best,

    Jieru

  • Hi Jieru,

    Certainly, they are available online at this link: https://www.ti.com/lit/zip/slwc115 

    Once you run the .exe, the files should install at this directory: C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\Source Code

    Regards, Chase