Part Number: DAC8718
Hello,
I am trying to use the DAC8718SPAG in a dual-supply configuration (+5V AVdd, -5V AVss, +2.5V REF, +3.3V IOVdd ). I also have RSTSEL pin tied to IOVdd and USB/BTC pin tied to ground. My understanding is that the DAC should detect that it is using a bipolar supply and set an appropriate 'Offset DAC-A/B' register value of 999Ah. The DACs in my system with this configuration are starting with an offset of 0000h and a DAC data value of 8000h. This would correspond to detecting a unipolar supply with my configuration of RSTSEL and USB/BTC pins. Could I please get clarification on how this DAC detects the bipolar supply? Am I possibly not meeting some voltage threshold or is there a further configuration needed to select bipolar supply?