Hi
I am using MSP430F5438 and ADS1258 and i can read and write the registers inside the ADS1258.I have setup the following register
Config0 = 0x2A ...Fixed Channel Mode,Clock ouptut on CLKIO enabled and Status byte enabled
Config1=0x00 ...Standy mode,No delay ,DRATE[1:0]=0x00
MUXSCH=0x11 Select AINP0 and AINN0
I am switching on the START line and keeping it high but i do not see and DRDY line going low .Am i suppose to do something in between the START and DRDY?
Thanks