Looking at the data sheet for the DAC1220, there is a power level given for 0-5V / 20 bit mode as 3 mW. However, the table says the main clock rate is 2.5 MHz.
1. What is the power if the main clock is 1 MHz or the lower limit of 500 kHz?
2. Also does this 3 mW include 250 kS/s update rate on the device or at a quiescent DC value (no serial interface clocking / updating DAC)?
3. Finally, is the power lower when it is at 25°C rather than from Tmin to Tmax? (If so, how much.) This is for lab environment with hard power metrics so I need to squeak as little power as possible.
Any help would be appreciated.
thanks,
David