Hi everybody,
I'm using the ADS1158 with AT91SAM9261 ARM microcontroller. I designed the first prototype board and it is working properly still now.
In the second board release the part of the circuit related to the ADC has not been changed (except litle layout modifications) as well as the SW release, but the SPI interface is not working at all in the new board.
I have checked the PCB in order to verify any short circuit and the result was nothing. I have checked A/D power supply, Vref and GNDs and it's all ok.
We have tried to to read the ID but unsuccessfully.
We have considered the possibility of a broken component and we have tried to change the component but with the same results.
The START pin is driven low and the /DRDY pin goes hight on power-up.
We use the Pulse Convert Command to start conversion and read channels
The configuration of the component is:
AVDD = 5V
DVDD = 5V
Vref = 4.096V
internal clock (32.768KHz quarz)
16 channels Single ended
Has anybody something to suggest or similar experiences. All suond as the component is broken but I checked the board with the inputs unconnected.
Many thanks for your help
Francesco