Do TI have DAC input from I2C and 4-20mA output?
Best Regards,
NT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do TI have DAC input from I2C and 4-20mA output?
Best Regards,
NT
Hi NT,
The DAC8750 is a DAC + XTR device which will give you 4-20mA output. The only problem you may run into is that it is SPI. It is due out with a month or two. If interested, let me know and we can get you a preliminary data sheet.
Regards,
Tony Calabria
Hi Tony,
My company is very much interested in the same. Can we a soft copy of the same?
Hi NT,
I am a bit late to this conversation, but I will use it as my practice run :)
You may want to check out DAC161P997 - you can do a search on it at ti.com.
It is a DAC built specifically for the isolated 4-20mA loop powered transmitters (Type-2 only).
It has a SWIF interface, even more stingy on wiring than i2c - just one wire needed to communicate with it, which is nice if you have to jump isolation boundary with your DAC input data.
Cheers!
tom