Part Number: ADS124S08
Per the ADS124S08 datasheet - it is recommended to tie REFCOM to AVSS when using the internal reference.
I am currently using this design with AVDD=2.625 and AVSS=-2.625 supplies and it would be useful instead of trying REFCOM to AVSS I could tie it to ground - so that relative to the rest of the board, REFOUT is +2.5V rather than -0.125V.
Is this a supported configuration of the device? Is the reason for the recommendation to tie to AVSS to ensure that there is enough headroom from REFCOM to AVSS, just a recommendation for a low, quiet voltage to tie it to, a requirement due to some internal protection circuits, or something else?
Thanks,
Drew