Part Number: DAC60508
Hi Team,
VDD and VIO same supply 3.3V
CS has 10K to VDD
No MOSI from chip to be able to read
REF to 2.2uF cap to gnd
SPI clk mode 1
after a reset the default register set seems to be enabled thru the SYNC reg addr 02 - 0xFF00 (async)
Gain reg is at reset all zeros -- I also tried setting it.
I set the DAC reg (8-F) to various 12bit value and never see the output turn on. (sync reg states that value is pushed out auto to the output reg.
I have tried various ways with the FSBO bit set/unset but shouldn't matter as there is NO SDO
All 24bit accesses are continuous with no byte gap
Hoping for your assistance.
Thank you.
-Mark