Part Number: ADS4249
Hi Experts,
Good day.
Our customer is using the ADS4249 for one of our applications and wants to use it in LVCMOS mode at a 180 MSPS sampling rate. They need clarity about the following.
1.In IBIS, for cmos_data_high1, currents are given in terms of typ, max & min. The actual ADS4249 represents which current (typ/max/min) because we do not have any option to select high drive strength for the CMOS data line. And whether 'typ' case is safer to consider for our IBIS simulations for our board?
2. Any flow charts or APIs are available to know about the programming sequences of ADC?
Keep safe.
Regards,
Josel